EtherCAT Implementation
- EtherCAT only uses standard Ethernet Ethernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) frames according to IEEE 802.3.
- EtherCAT slave controllers are used where such dedicated chips really make sense: in the slave device.
- They handle the process data protocol in hardware and provide maximum real-time performance regardless of the local processing power or software quality.